:WMEMory:TTIMebase
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:TTIMebase {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:TTIMebase?
Query Response
{1 | 0}
Description
Turns the track timebase function on and off. With track timebase on, the time scale and position of the displayed waveform memory is set to and tracks the time scale and position settings made in the :TIMebase subsystem (:TIMebase:SCALe and :TIMebase:POSition).