:WMEMory:WINTerp
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:WINTerp {NONE | LINear | SINC}
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:WINTerp?
Description
Specifies the type of interpolation applied between the points to make measurements when waveform wrapping is applied (:WMEMory:WRAPping). This command is available whenever color-grade or gray-scale persistence is turned on (:DISPlay:PERSistence). These types of persistence are always used in Eye/Mask mode.
- LINear
- Selects linear interpolation.
- SINC
- Selects Sin(x)/x interpolation.
- NONE
- Turns interpolation off.