:WMEMory:STATus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Query Syntax
:WMEMory{1:8}:STATus?
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Response
{AVA | UNAV}
Description
Queries the availability of a waveform memory for use. Waveform memory becomes available (AVA) after data has been loaded into it using the :WMEMory:LOAD command. The waveform memory does not need to be displayed to be classed as available. Available Waveform memories are shown in the Signals Palette. A Waveform memory is unavailable (UNAV) if no data has been loaded into the memory.
Use the :WMEMory:DISPlay command query to determine if a waveform memory waveform is displayed.