:WMEMory:SRATe
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:SRATe symbol_rate
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
<symbol_rate> is a double.
Query Syntax
:WMEMory{1:8}:SRATe?
Description
Enters the symbol rate used, which automatically sets the unit-interval range :TIMebase:UIRange and unit-interval delay :TIMebase:UIPosition. To change the timebase scale to seconds instead of unit interval, use :TIMebase:UNITs.
In Jitter Mode, symbol rate, unit intervals displayed, and unit interval delay controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :WMEMory:BRATe.
Example Command Sequence
:TIMebase:UNITs BIT :TIMebase:SRATe 9.953E+9