:TPRogram:SLINe:EDIMage:IMETadata
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:EDIMage:IMETadata {ON | OFF}
Query Response
{0 | 1}
Description
For a Station's selected Test Program line, embeds metadata into an image when an eye diagram is saved to a JPEG or TIFF image file. The command is equivalent to the Include Metadata field in the Selected Test Line Setup dialog. This setting is on by default.
To specify that an image be saved with the measurement results, add the EDIMage argument to the :TPRogram:SLINe:MEASurements command. When adding new lines to a Test Program, use the :TPRogram:SETup:EDIMage:FTYPe command.
The metadata data that is embedded includes information such as:
- CreatorTool: "FlexOTO (P.07.XX.XXX)"
- CreateDate: "2023-09-21T10:07:20"
- Make: "Keysight Technologies"
- Model: "FlexOTO (P.07.XX.XXX)"