:TPRogram:SLINe:ENABle
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SLINe:ENABle {ON | OFF}
Query Syntax
:TPRogram:SLINe:ENABle?
Query Response
{1 | 0}
Description
Includes or excludes the selected Test Program line from being run with the Test Program. You must first select the Test Program line using the :TPRogram:SLINe:INDex command. By default, all the lines that are added to a Test Program are set to be included. This commands lets you omit lines in a Test Program without having to alter the Test Program.