:TPRogram:SLINe:SRATe
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Symbol Rate Selections
Availability of individual rates depends on installed modules and other conditions.
- 51.84 MBd - STM-0/OC-1
- 125.0 MBd - FDDI/100M Ethernet
- 155.52 MBd - STM-1/OC-3
- 270.0 MBd - SDI
- 614.4 MBd - CPRI
- 622.08 MBd - STM-4/OC-12
- 768.00 MBd - OBSAI
- 1.06250 GBd - 1G Fibre Channel
- 1.22880 GBd - CPRI 2x
- 1.244160 GBd - GPON/OC-24
- 1.25000 GBd - Gb Ethernet
- 1.48500 GBd - SDI
- 1.50000 GBd - SATA-1/SAS-1
- 1.53600 GBd - OBSAI 2x
- 2.12500 GBd - 2B Fibre Channel
- 2.4576 GBd - CPRI 4x
- 2.48832 GBd - STM-16/OC-48
- 2.50000 GBd - PCIe1/2 Gb Ethernet/InfiniBand
- 2.6660570 GBd - STM-16/OC-48 FEC
- 2.97000 GBd - SDI
- 3.00000 GBd - SATA-2/SAS-2
- 3.07200 GBd - CPRI 5x / OBSAI 4x
- 3.12500 GBd - XAUI / 10GbE Base-LX4
- 3.18750 GBd - FC-3187/10GBE Base-LX4
- 3.25000 GBd - Rapid IO
- 3.32000 GBd - 12x Parallel Optics
- 4.25000 GBd - 4G Fibre Channel
- 4.9152 GBd - CPRI 8x
- 5.00000GBd - PCIe-2/2x InfiniBand
- 6.00000 GBd - SATA-3/SAS3/CEI
- 6.144 GBd - CPRI 10X / OBSAI 8X
- 6.25000 GBd - 2x XAUI
- 6.37500 GBd - CEI 6G+
- 8.00000 GBd - PCIe-3
- 8.1100800 GBd - CPRI 16x
- 8.50000 GBd - 8x Fibre Channel
- 9.8304 GBd - CPRI 16x
- 9.95328 GBd - STM-64/OC-192/10GbEthernet
- 10.00 GBd - InfiniBand QDR
- 10.1376 GBd - CPRI 20x
- 10.3125 GBd - 10Gb Ethernet LR/ER
- 10.51875 GBd - 10G Fibre Chanel
- 10.664230 GBd - STM-64/OC-192 FEC
- 10.7090 GBd - STM-64/OC-192 FEC
- 11.0000 GBd - CEI 11G
- 11.0957 GBd - 10Gb Ethernet FEC
- 11.3170 GBd - 10GFC FEC
- 12.165120 GBd - CPRI 24x
- 12.249450 GBd - STM-64/OC-192 SuperFEC
- 12.44160000 GBd - ITU-T PON
- 14.025000 GBd - 16G Fibre Channel
- 14.06250 GBd - InfiniBand FDR
- 16.00000 GBd - PCIe-4
- 24.33024000 GBd - CPRI 48x
- 24.88320000 GBd - ITU-T PON
- 25.78125 GBd - 100GbE/4 / InfiniBand EDR
- 26.56250000 GBd - 400GBASE-SR16
- 27.7393 GBd - 100Gb Ethernet / 4 FEC
- 27.952493 GBd - OTU4/ITU-T G.959.1
- 28.05 GBd - 32G Fibre Channel
- 28.9 GBd - 64G Fibre Channel
- 32.00000 GBd - PCIe-5/PCIe-6
- 39.81312 GBd - STM-256/OC-768
- 41.250000 GBd - 40Gb Ethernet
- 43.018413 GBd - STM-256/OC-768 FEC
- 49.76640000 GBd - ITU-T PON
- 53.125 GBd - 400GBASE
- 56.100000 GBd - 128G Fibre Channel
- 79.626240 GBd - STM-512/OC-1536
- 106.25000 GBd - 800GBASE
- 112.50000 GBd - 4x200G-FR4
- 113.34570 GBd - 800GBASE (FECi)
- 115.10417 GBd -
- 159.25248 GBd - STM-1024/OC-3072
Command Syntax
:TPRogram:SLINe:SRATe <symbol-rate>
The symbol rate is a double. For example, 5.3225000E+10.
Query Syntax
:TPRogram:SLINe:SRATe?
Query Response
<symbol-rate>
Description
For a Station's selected Test Program line, changes the applied Symbol Rate.
Example
station.write(':TPRogram:SLINe:SRATe 26.5625E+9')