:TPRogram:SLINe:LDEFinition

Flex Apps:
FlexOTO
FlexOTO Instance:
Stations

Command Syntax

:TPRogram:SETup:LDEFinition {RLMA120 | RLMC94 | EYE}

Query Response

{RLMA120 | RLMC94 | EYE}

Description

For a Station's selected Test Program line, selects the Linearity Definition based on RLM (Ratio Level Mismatch) or Eye Linearity. This definition is applied to FlexOTO's Linearity measurement. The available definitions are:

RLMA120
RLM (IEEE 802.3 Annex 120D). This is the default definition.
RLMC94
RLM (IEEE 802.3 Clause 94)
EYE
Eye Linearity (CEI 4.0)

When adding new lines to a Test Program, use the :TPRogram:SETup:LDEFinition command.

Measurements Affected by Configuration Settings (PAM4 Waveform)
Measurement Power Units Outer ER Units Linearity Definition Target Transition Target Hit Ratio
:TPRogram:SLINe:PUNits :TPRogram:SLINe:ERUNits :TPRogram:SLINe:LDEFinition :TPRogram:SLINe:TRANsition :TPRogram:SLINe:THRatio
Average Power ■
Ceq Noise Gain
Levels ■
Linearity ■
Outer ER ■
Outer OMA ■
Overshoot ■
Peak-Peak Power ■
TDECQ
Transition Time ■
Tx Power Excursion ■ ■
Undershoot ■