:TPRogram:SLINe:FIXTure
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SLINe:FIXTure ,"<fixture-name>"
Where <fixture-name> is a name string that identifies the DUT Fixture or WDM DUT Fixture block on the Hardware Diagram. Be sure to include the double quote (") characters in the string. The string can include up to 20 valid Windows file name characters.
Query Response
<fixture-name>
Description
When editing an existing line in a Test Program, use this command to change the assigned fixture. You must first select the line using the :TPRogram:SLINe:INDex command. The :TPRogram:SLINe:FIXTure command is equivalent to the Fixture field in the Selected Test Lne Setup dialog.