:TPRogram:SLINe:EDIMage:SRESults
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SLINe:EDIMage:SRESults {ON | OFF}
Query Response
{0 | 1}
Description
For a Station's selected Test Program line, specifies whether the measurements results will be rasterized and embedded as part of the eye diagram image. In addition to setting this command, be sure to select that an image be saved by appending the EDIMage argument to the :TPRogram:SLINe:MEASurements command.