:TPRogram:SLINe:IMPairments
Command Syntax
:TPRogram:SLINe:IMPairments ["impairment-name,impairment-name,impairment-name,..."]
Where <impairment-name> is a name string that identifies an Impairment block on the Hardware Diagram. Be sure to include the double quote (") characters on both sides of the entire string. The string can include up to 20 valid Windows file name characters.
Query Syntax
:TPRogram:SLINe:IMPairments?
Query Response
"impairment-name,impairment-name,impairment-name,..."
A comma delimited string of all Impairments selected to be included in the Test Program.
Description
When editing an existing line of a Test Program, this command selects one or more Impairments to be included in the Test Program. This command is equivalent to the Impairments settings field in the Test Program Measurement Setup dialog.
To disable all Impairments from the Test Plan line, send this command without any arguments.
To include Impairments when creating new lines of a Test Program, use the :TPRogram:SETup:IMPairments command.