Note: Beginning with Revision 4.0, the following data analysis features are available separately as part of PLTS Studio -- an analysis-only software package.
The following topics discuss all aspects of PLTS Data Analysis:
About Windows,Plots, and Traces
Data Format and Scale
Markers
Math
Limit Lines
Statistical Equation Traces
Data Integrity Check
Templates
MatLab Equations
Python Equations
Multi-channel Eye Diagrams
Standard Views
Analyzing Data in the Frequency Domain
Analyzing Data in the Time Domain
Analyzing Data using Eye Diagrams
Eye Diagram Bit Patterns
Eye Diagram Mask Testing
Multi-channel Simulation
Pre/DeEmphasisExample
Synthesize Eye Diagram from Equations
Analyzing Transmission Line Parameters