:CHANnel:CRECovery:CEIDle
Command Syntax
:CHANnelN:CRECovery:CEIDle {ON | OFF | 1 | 0}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:CRECovery:CEIDle?
Description
Enables or disables the Contains Electrical Idle option.
When you are decoding a serial bus that has bursts of serial data followed by long periods of idle time, enabling the Contains Electrical Idle control will remove idle time from the decoded serial data.
To specify the Idle Clock Count, use :CHANnel:CRECovery:ICCount.