:CHANnel:CRECovery:SOPLl:JTF:LBANdwidth
Command Syntax
:CHANnelN:CRECovery:SOPLl:JTF:LBANdwidth <loop_bandwidth>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<loop_bandwidth> is a double.
Query Syntax
:CHANnelN:CRECovery:SOPLl:JTF:LBANdwidth?
Description
Specifies the PLL's loop bandwidth (also known as the -3 dB BW).
Example Command Sequence
:CHANnel1:CRECovery:MODE SOPLl :CHANnel1:CRECovery:PLL:MODE JTF :CHANnel1:CRECovery:SOPLl:JTF:LBANdwidth 2.837E+6 :CHANnel1:CRECovery:SOPLl:JTF:PEAKing 1.25