:CHANnel:CRECovery:ECLock:CFRequency

Command Syntax

:CHANnelN:CRECovery:ECLock:CFRequency <frequency>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<frequency> is a real number used for the clock frequency of the PLL.

Query Syntax

:CHANnelN:CRECovery:ECLock:CFRequency?

Description

With the Explicit 1st or 2nd Order PLL clock recovery methods (see :CHANnel:CRECovery:MODE), this command specifies the clock frequency of the PLL.

Example Command Sequence

:CHANnel1:CRECovery:MODE EFOPll
:CHANnel1:CRECovery:ECLock:CFRequency 1.485E+09