:CHANnel:CRECovery:SRATe:STATus:REASon?
Query Syntax
:CHANnelN:CRECovery:SRATe:STATus:REASon?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for a failed :CHANnel:CRECovery:SRATe measurement. If the measurement was successful, a null string is returned.
Use the :CHANnel:CRECovery:SRATe:STATus? parent query to determine if the measurement has failed.