:CHANnel:CRECovery:SOPLl:OJTF:LBANdwidth

Command Syntax

:CHANnelN:CRECovery:SOPLl:OJTF:LBANdwidth <loop_bandwidth>
            

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<loop_bandwidth> is a double.

Query Syntax

:CHANnelN:CRECovery:SOPLl:OJTF:LBANdwidth?

Description

Specifies the PLL's loop bandwidth (also known as the -3 dB BW).

Example Command Sequence

:CHANnel1:CRECovery:MODE SOPLl
:CHANnel1:CRECovery:PLL:MODE OJTF
:CHANnel1:CRECovery:SOPLl:OJTF:LBANdwidth 1.779E+6
:CHANnel1:CRECovery:SOPLl:OJTF:DFACtor 0.707