:CHANnel:CRECovery:TRACking

Command Syntax

:CHANnelN:CRECovery:TRACking {ON | OFF | 1 | 0}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:CRECovery:TRACking?

Query Response

{1 | 0}

Description

Specifies whether the channel's clock recovery settings should track (use) the global settings or use custom settings specific to this waveform.

When using the global settings, see :CRECovery Subsystem commands.

When using custom settings specific to this waveform, see :CHANnel CRECovery Commands.