:CHANnel:CRECovery:SOPLl:JTF:PEAKing

Command Syntax

:CHANnelN:CRECovery:SOPLl:JTF:PEAKing <peaking_in_dB>
            

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<peaking_in_dB> is a double.

Query Syntax

:CHANnelN:CRECovery:SOPLl:JTF:PEAKing?

Description

When specifying the PLL's loop bandwidth in terms of the JTF 3 dB BW, you also need to specify the peaking of the JTF.

Example Command Sequence

:CHANnel1:CRECovery:MODE SOPLl
:CHANnel1:CRECovery:PLL:MODE JTF
:CHANnel1:CRECovery:SOPLl:JTF:LBDivisor 1.047E+3
:CHANnel1:CRECovery:SOPLl:JTF:PEAKing 1.25