:CHANnel:CRECovery:FOPLl:LBDivisor

Command Syntax

:CHANnelN:CRECovery:FOPLl:LBDivisor <loop_bandwidth_divisor>
            

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<loop_bandwidth_divisor> is a double.

Query Syntax

:CHANnelN:CRECovery:FOPLl:LBDivisor?

Description

Specifies a number that the symbol rate is divided by to get the loop bandwidth.

Example Command Sequence

:CHANnel1:CRECovery:MODE FOPLl
:CHANnel1:CRECovery:FOPLl:LBDivisor 1.667E+3