:CHANnel:CRECovery:ZOPLl:SPOLe
Command Syntax
:CHANnelN:CRECovery:ZOPLl:SPOLe <secondary_pole_frequency>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<secondary_pole_frequency> is a double.
Query Syntax
:CHANnelN:CRECovery:ZOPLl:SPOLe?
Description
Specifies the fifth-order PLL's secondary pole frequency, ω1, which is an angular frequency in radians/sec. ω is equivalent to 2πf, where f is frequency in Hertz.
Example Command Sequence
:CHANnel1:CRECovery:MODE ZOPLl :CHANnel1:CRECovery:ZOPLl:SPOLe 24.38E+06