:CHANnel:CRECovery:SRATe:STATus?
Query Syntax
:CHANnelN:CRECovery:SRATe:STATus?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the :CHANnel:CRECovery:SRATe measurement. Use the :CHANnel:CRECovery:SRATe:STATus:REASon? child query to determine the reason for an invalid or questionable measurement