:CHANnel:CRECovery:PLL:EDIRection
Command Syntax
:CHANnelN:CRECovery:PLL:EDIRection {RISing | FALLing | BOTH}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:CRECovery:PLL:EDIRection?
Description
Specifies the signal edge(s) to use when recovering a clock. Typically, for all clock recovery methods except Explicit, you would use BOTH edges of a signal to recover a clock. However, the other options are available if, for example, the signal is a clock signal with a low duty cycle and you want to measure jitter only on its rising (or falling) edges.
Example Command Sequence
:CHANnel1:CRECovery:MODE FOPLl :CHANnel1:CRECovery:PLL:EDIRection BOTH