:CHANnel:CRECovery:SOPLl:OJTF:DFACtor
Command Syntax
:CHANnelN:CRECovery:SOPLl:OJTF:DFACtor <damping_factor>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<damping_factor> is a double.
Query Syntax
:CHANnelN:CRECovery:SOPLl:OJTF:DFACtor?
Description
When specifying the PLL's loop bandwidth in terms of the OJTF 3 dB BW, you also need to specify the damping factor of the JTF.
| < 1 | underdamped |
| > 1 | overdamped |
| = 1.0 | critically damped |
| = 0.707 | Often considered ideal or optimal because of its fast settling time (optimally flat) and Butterworth type response. |
Example Command Sequence
:CHANnel1:CRECovery:MODE SOPLl :CHANnel1:CRECovery:PLL:MODE OJTF :CHANnel1:CRECovery:SOPLl:OJTF:LBDivisor 1.670E+3 :CHANnel1:CRECovery:SOPLl:OJTF:DFACtor 0.707