:CHANnel:CRECovery:SRATe:STATus:DETails?
Query Syntax
:CHANnelN:CRECovery:SRATe:STATus:DETails?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
If the status of the clock recovery symbol rate is questionable or invalid (see :CHANnel:CRECovery:SRATe:STATus?), this query returns a string that may provide additional details.
If the status of the clock recovery symbol rate is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :CHANnel:CRECovery:SRATe:STATus:REASon? sibling query.