:CHANnel:CRECovery:FOPLl:LBANdwidth
:CHANnel CRECovery Commands
- :CHANnel CRECovery Commands
- :CHANnel:CRECovery:CEALgorithm
- :CHANnel:CRECovery:CEIDle
- :CHANnel:CRECovery:CFRequency:EDIRection
- :CHANnel:CRECovery:CFRequency:MODE
- :CHANnel:CRECovery:CSKew
- :CHANnel:CRECovery:CSRate?
- :CHANnel:CRECovery:DDRFive:CAFLatency
- :CHANnel:CRECovery:DDRFive:CAFSource
- :CHANnel:CRECovery:DDRFive:DQSSource
- :CHANnel:CRECovery:DDRFive:POLength
- :CHANnel:CRECovery:DDRFive:PRLength
- :CHANnel:CRECovery:DDRFive:RWMode
- :CHANnel:CRECovery:DDRFive:STDDelay
- :CHANnel:CRECovery:DREMoval
- :CHANnel:CRECovery:ECLock:ALIGn
- :CHANnel:CRECovery:ECLock:CFRequency
- :CHANnel:CRECovery:ECLock:CMULtiplier
- :CHANnel:CRECovery:ECLock:DELay
- :CHANnel:CRECovery:ECLock:EDIRection
- :CHANnel:CRECovery:ECLock:SOURce
- :CHANnel:CRECovery:FOPLl:LBANdwidth
- :CHANnel:CRECovery:FOPLl:LBDivisor
- :CHANnel:CRECovery:FSRate
- :CHANnel:CRECovery:ICCount
- :CHANnel:CRECovery:MODE
- :CHANnel:CRECovery:PLL:EDIRection
- :CHANnel:CRECovery:PLL:MODE
- :CHANnel:CRECovery:PLL:SSCCorrect
- :CHANnel:CRECovery:PLL:SSPercent
- :CHANnel:CRECovery:PLL:SSType
- :CHANnel:CRECovery:PLL:STIMe
- :CHANnel:CRECovery:PLL:TDEPendent
- :CHANnel:CRECovery:PRESets
- :CHANnel:CRECovery:PRESets:SELections?
- :CHANnel:CRECovery:SOPLl:JTF:LBANdwidth
- :CHANnel:CRECovery:SOPLl:JTF:LBDivisor
- :CHANnel:CRECovery:SOPLl:JTF:PEAKing
- :CHANnel:CRECovery:SOPLl:OJTF:DFACtor
- :CHANnel:CRECovery:SOPLl:OJTF:LBANdwidth
- :CHANnel:CRECovery:SOPLl:OJTF:LBDivisor
- :CHANnel:CRECovery:SRATe
- :CHANnel:CRECovery:SRATe:STATus?
- :CHANnel:CRECovery:SRATe:STATus:DETails?
- :CHANnel:CRECovery:SRATe:STATus:REASon?
- :CHANnel:CRECovery:TOPLl:DFACtor
- :CHANnel:CRECovery:TOPLl:NFReq
- :CHANnel:CRECovery:TOPLl:PFReq
- :CHANnel:CRECovery:TRACking
- :CHANnel:CRECovery:ZOPLl:LFPole
- :CHANnel:CRECovery:ZOPLl:PPOLe
- :CHANnel:CRECovery:ZOPLl:SPOLe
Command Syntax
:CHANnelN:CRECovery:FOPLl:LBANdwidth <loop_bandwidth>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<loop_bandwidth> is a double.
Query Syntax
:CHANnelN:CRECovery:FOPLl:LBANdwidth?
Description
Specifies the PLL's loop bandwidth (also known as the -3 dB BW).
Example Command Sequence
:CHANnel1:CRECovery:MODE FOPLl :CHANnel1:CRECovery:FOPLl:LBANdwidth 1.782E+6