:CHANnel:CRECovery:PLL:STIMe
Command Syntax
:CHANnelN:CRECovery:PLL:STIMe <settling_time>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<settling_time> is a double.
Query Syntax
:CHANnelN:CRECovery:PLL:STIMe?
Description
Specifies the settling time as a number of time constants. All PLLs take a finite amount of time to lock on to their source signal. During this settling time portion of the acquisition record, jitter measurements, protocol decode, etc. will not be performed.
Example Command Sequence
:CHANnel1:CRECovery:MODE FOPLl :CHANnel1:CRECovery:PLL:STIMe 5.0