:CHANnel:CRECovery:SOPLl:JTF:LBDivisor
Command Syntax
:CHANnelN:CRECovery:SOPLl:JTF:LBDivisor <loop_bandwidth_divisor>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<loop_bandwidth_divisor> is a double.
Query Syntax
:CHANnelN:CRECovery:SOPLl:JTF:LBDivisor?
Description
Specifies a number that the symbol rate is divided by to get the loop bandwidth.
Example Command Sequence
:CHANnel1:CRECovery:MODE SOPLl :CHANnel1:CRECovery:PLL:MODE JTF :CHANnel1:CRECovery:SOPLl:JTF:LBDivisor 1.047E+3 :CHANnel1:CRECovery:SOPLl:JTF:PEAKing 1.25