:CHANnel:CRECovery:PLL:SSCCorrect
Command Syntax
:CHANnelN:CRECovery:PLL:SSCCorrect {ON | OFF | 1 | 0}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:CRECovery:PLL:SSCCorrect?
Description
Lets you enable or disable the application of SSC (spread-spectrum clocking) correction. This information improves the performance of clock recovery.
When enabled:
-
Use the
:CHANnel:CRECovery:PLL:SSTypecommand to specify the type of SSC being used. -
Use the
:CHANnel:CRECovery:PLL:SSPercentcommand to specify the magnitude of the symbol rate change (spread) as a percent.