:CHANnel:CRECovery:PLL:ICCount

Command Syntax

:CHANnelN:CRECovery:PLL:ICCount <idle_clock_count>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<idle_clock_count> is an integer from 10 to 200.

Query Syntax

:CHANnelN:CRECovery:PLL:ICCount?

Description

Specifies the number of clock periods without a data transition (edge) that indicate an idle condition. This option lets protocol decoders suppress decode for idle data periods on serial data links that go quiescent for a period of time and then restart transmitting.

Example Command Sequence

:CHANnel1:CRECovery:MODE FOPLl
:CHANnel1:CRECovery:PLL:ICCount 80