:PROTocol:PROTocol:BORDer

Command Syntax

:PROTocol:PROTocolN:BORDer  {<depends_on_protocol_type>}

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Query Syntax

:PROTocol:PROTocolN:BORDer?

Description

Depending on the selected :PROTocol:PROTocol:TYPE, this command specifies the bit order. It can be either most significant bit first (MSB) or least significant bit first (LSB).

Display formats available for protocol types
Protocol type Display formats
G8B10B {MSB}
GRAW {MSB}
USB4 {MSB}