:PROTocol:PROTocol:NSOurces

Command Syntax

:PROTocol:PROTocolN:NSOurces  <num_sources>

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Where <num_sources> is an integer from one to four.

Query Syntax

:PROTocol:PROTocolN:NSOurces?

Description

Depending on the selected :PROTocol:PROTocol:TYPE, this command specifies the number of sources to use in the protocol decode. There is a maximum number of four sources.

Number of sources available for protocol types
Protocol type Possible number of sources
G8B10B 1-4
GRAW 1

You can query the name of a source using :PROTocol:PROTocol:SOURce:NAME?.