:PROTocol:PROTocol:DFORmat

Command Syntax

:PROTocol:PROTocolN:DFORmat  {<depends_on_protocol_type>}

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Query Syntax

:PROTocol:PROTocolN:DFORmat?

Description

Depending on the selected :PROTocol:PROTocol:TYPE, this command specifies the displayed format of the decoded values. The default setting is HEX.

Display formats available for protocol types
Protocol type Display formats
G8B10B {HEX | DECimal | BINary}
GRAW {HEX | DECimal | BINary | ASCii}