:PROTocol:PROTocol:SOURce:LSEed

Command Syntax

:PROTocol:PROTocolN:SOURceS:LSEed  {SING0 | MULT0 | MULT1 | MULT2}

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Where S identifies one of four possible source waveforms {1:4} that contribute to the protocol. For example, :PROTocol:PROTocol3:SOURce1. The possible number of source waveforms, :PROTocol:PROTocol:NSOurces, depends on the selected :PROTocol:PROTocol:TYPE.

Query Syntax

:PROTocol:PROTocolN:SOURceS:LSEed?

Description

This command determines the default descrambling seed to be used for this lane. For example, if MULT0 is selected, the default descrambling seed is the one defined in the specification for Lane 0 in a multi-lane configuration.

  • SING0 — This source is a single lane (not part of multiple lanes).

  • MULT0 — This source is Lane 0 of a multi-lane decode.

  • MULT1 — This source is Lane 1 of a multi-lane decode.

  • MULT2 — This source is Lane 2 of a multi-lane decode. (Lane 2 can be present in USB4v2 Asymmetric mode.)