:PROTocol:PROTocol:PLISting:INDex:MIN?
Query Syntax
:PROTocol:PROTocolN:PLIStingL:INDex:MIN?
Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.
Where L identifies one of four possible packet listings {1:4} if the protocol decode has multiple listings. For example, PLISting2.
Description
When acquisitions are stopped (see :ACQuire:STOP), this query returns the lowest row index number in the protocol packet listing.
You can use the :PROTocol:PROTocol:PLISting:INDex:MAX? query to get the highest row index number.
You can use the :PROTocol:PROTocol:PLISting:INDex command to navigate to protocol packet listing rows between the lowest and the highest row index numbers.