:PROTocol:PROTocol:SLISting:INDex:MIN?

Query Syntax

:PROTocol:PROTocolN:SLIStingL:INDex:MIN?

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Where L identifies one of four possible symbol listings {1:4} if the protocol decode has multiple listings. For example, SLISting2.

Description

When acquisitions are stopped (see :ACQuire:STOP), this query returns the lowest row index number in the protocol symbol listing.

You can use the :PROTocol:PROTocol:SLISting:INDex:MAX? query to get the highest row index number.

You can use the :PROTocol:PROTocol:SLISting:INDex command to navigate to protocol symbol listing rows between the lowest and the highest row index numbers.