:PROTocol:PROTocol:SEARch:FIELd:PAYLoad:WORD:SYMBol
Command Syntax
:PROTocol:PROTocolN:SEARch:FIELdF:PAYLoad:WORDW:SYMBol{1|2} <quoted_string>
Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.
Where F identifies one of three possible fields {1:3}. For example, FIELd2.
Where W identifies one of 32 possible words {1:32}. For example, WORD2.
Query Syntax
:PROTocol:PROTocolN:SEARch:FIELdF:PAYLoad:WORDW:SYMBol{1|2}?
Description
When specifying search values using K Codes (see :PROTocol:PROTocol:SEARch:FIELd:PAYLoad:WORD:TYPE), for the specified word in the field's payload, this command specifies the symbol value. You can use: "Any", "K28.0", "K28.1", "K28.2", "K28.3", "K28.4", "K28.5", "K28.6", "K28.7", "K23.7", "K27.7", "K29.7", or "K30.7".
With the EQUal operator (see ), you specify the single word value using the :PROTocol:PROTocolN:SEARch:FIELd:PAYLoad:WORDW:SYMBol or :PROTocol:PROTocolN:SEARch:FIELd:PAYLoad:WORDW:SYMBol1 command.
With the OR operator, you specify two word values using the :PROTocol:PROTocolN:SEARch:FIELd:PAYLoad:WORDW:SYMBol1 and :PROTocol:PROTocolN:SEARch:FIELd:PAYLoad:WORDW:SYMBol2 commands.