:PROTocol:PROTocol:STATus:DETails?

Query Syntax

:PROTocol:PROTocolN:STATus:DETails?

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Description

Returns a string that may provide additional details for a questionable or invalid protocol decode. If the protocol decode is correct, a null string is returned.

For a basic description of a questionable or invalid protocol decode, use the :PROTocol:PROTocol:STATus:REASon? sibling query. Use the :PROTocol:PROTocol:STATus? parent query to determine if the decode is questionable or invalid.

See Also