:PROTocol:PROTocol:COPY

Command Syntax

:PROTocol:PROTocolN:COPY

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Description

For the selected protocol decode, this command will copy the protocol qualified trigger setup to its search setup.

For more information on setting up protocol qualified triggers, see :TRIGger Qualify Commands.