:PROTocol:PROTocol:PRECoding

Command Syntax

:PROTocol:PROTocolN:PRECoding  {OFF | ON}

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Query Syntax

:PROTocol:PROTocolN:PRECoding?

Description

Depending on the selected :PROTocol:PROTocol:TYPE, this command enables or disables precoding.

This command can be used with the following protocol types:

  • USB4