:PROTocol:PROTocol:SFORmat

Command Syntax

:PROTocol:PROTocolN:SFORmat {<depends_on_protocol_type>}

Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.

Query Syntax

:PROTocol:PROTocolN:SFORmat?

Description

Depending on the selected :PROTocol:PROTocol:TYPE, this command specifies the symbol format to use in the decode.

For the G8B10B protocol type, you can specify:

  • LABel — Defined labels are displayed.

    When LABel is selected, if no label is defined for the value (as is the case with K Codes), the K/D Code format (like "K28.0" for example) will be displayed.

  • KDCode — K/D Codes are displayed (like "K28.0" or "D28.3+" for example).

  • F8Bit — The 8-bit representation.

  • F10Bit — The 10-bit representation.