:TDR:DUT:DIFFerential:PPORt:UNAMe
Command Syntax
:TDR:DUT{1:16}:DIFFerential:PPORt{1:16}:UNAMe <string>
Where {1:16} indicates one of 16 possible DUT setups.
Where {1:16} indicates one of 8 possible DUT ports. For example, :PPORT2.
Query Syntax
:TDR:DUT{1:16}:SENDed:PPORt{1:8}:UNAMe?
Description
Replaces the default port signal label with custom user label for the selected +signal of a differential DUT. The channel, default port, and custom user signal labels are displayed in Waveform content windows as shown in the following table. The default port labels are Port 1+, Port 2+, …. Your custom user labels can be up to 25 characters long. To reset a custom user label to its default port label, send an empty string.
To enter custom user labels for differential –signals or port, use the following commands:
| ASNaming Command OFF | ASNaming Command ON | ||
|---|---|---|---|
| Default Port Labels |
Custom Labels | ||
| ADPNaming Command OFF (Custom Diff +/– Labels) |
ADPNaming Command ON (Custom Diff Port Labels) |
||
|
|
|
|
As shown in the above table, to select the labels to display use the following commands:
:TDR:ASNamingcommand:TDR:ADPNamingcommand to select the type of label that is displayed.
Custom user names can by created for other waveforms using the following commands:
:CHANnel:UNAMe:CMODe:UNAMe:DIFF:UNAMe:EMEMory:UNAMe:FUNCtion:UNAMe:TDR:DUT:DIFFerential:NPORt:UNAMe:TDR:DUT:DIFFerential:SIGNal:UNAMe:TRACe:UNAMe:WMEMory:UNAMe
Requires FlexDCA revision A.04.00 and above.