:TDR:DUT:DIFFerential:SIGNal:UNAMe
Command Syntax
:TDR:DUT{1:16}:DIFFerential:SIGNal{1:16}:UNAMe <string>
Where {1:16} indicates one of 16 possible DUT setups.
Where {1:16} indicates one of 8 possible DUT port signal labels. For example, :SIGNal2.
Query Syntax
:TDR:DUT{1:16}:SENDed:SIGNal{1:8}:UNAMe?
Description
Replaces the default port signal label with custom user label for the selected port of a differential DUT. The channel, default port, and custom user signal labels are displayed in Waveform content windows as shown in the following table. The default port labels are Port 1, Port 2, …. Your custom user labels can be up to 25 characters long. To reset a custom user label to its default port label, send an empty string.
To enter custom user labels for differential +/– signals, use the following commands:
| ASNaming Command OFF | ASNaming Command ON | ||
|---|---|---|---|
| Default Port Labels |
Custom Labels | ||
| ADPNaming Command OFF (Custom Diff +/– Labels) |
ADPNaming Command ON (Custom Diff Port Labels) |
||
|
|
|
|
As shown in the above table, to select the labels to display use the following commands:
:TDR:ASNamingcommand:TDR:ADPNamingcommand to select the type of label that is displayed.
Custom user names can by created for other waveforms using the following commands:
:CHANnel:UNAMe:CMODe:UNAMe:DIFF:UNAMe:EMEMory:UNAMe:FUNCtion:UNAMe:TDR:DUT:DIFFerential:NPORt:UNAMe:TDR:DUT:DIFFerential:PPORt:UNAMe:TRACe:UNAMe:WMEMory:UNAMe
Requires FlexDCA revision A.04.00 and above.