:MEASure:AMPLitude:DEFine:RINoise:TYPe
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
Command Syntax
:MEASure:AMPLitude:DEFine:RINoise:TYPe {OLEVel | OMA}
Query Syntax
:MEASure:AMPLitude:DEFine:RINoise:TYPe?
Description
Configures the Relative Intensity Noise (RIN) measurement (:AMPLitude:RINoise
) to be based on one of the following:
- OLEVel
- The one level.
- OMA
- The Optical Modulation Amplitude (OMA) measurement.
Additional definitions for the RIN measurement:
:MEASure:AMPLitude:DEFine:RINoise:DEFinition
to FlexDCA legacy or IEEE algorithm.:MEASure:AMPLitude:DEFine:RINoise:UNITs
to select the measurement units.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis
command.