:MEASure:AMPLitude:DEFine:RNComp
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:RNComp {OFF | AUTomatic | CUSTom}
Query Syntax
:MEASure:AMPLitude:DEFine:RNComp?
Query Response
{OFF | AUT | CUST}
Description
Selects the RN compensation which removes intrinsic oscilloscope noise from the measurement results. Use the following arguments.
OFF- RN compensation is turned off and measurements include the oscilloscope's intrinsic noise. The equivalent setting in the Jitter Mode Measurement Setup dialog's Advanced tab for RN Compensation is "Off".
AUTomatic- Oscilloscope intrinsic noise is removed from measurements. This should be the selection for RIN measurements on an optical signal. The equivalent setting in the Jitter Mode Measurement Setup dialog's Advanced tab for RN Compensation is "Remove Scope Noise".
CUStom- Deprecated. This selection is not recommended, but allows you to manually enter the RN one level and zero level compensation values with the deprecated
:MEASure:AMPLitude:DEFine:RNCValue:ONEand:MEASure:AMPLitude:DEFine:RNCValue:ZEROcommands. Depending on the type of signal that you are measuring enter the values in volts (electrical) or watts (optical). Estimate the Random Noise that is contributed by the N1000A by disconnecting all cables and signals from the oscilloscope's input and then measuring Vrms (AC) in Oscilloscope mode. The equivalent setting in the Jitter Mode Measurement Setup dialog's Advanced tab for RN Compensation is "Remove Custom Noise Values".
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.