:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LEADing

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LEADing  <digits>;

<digits> is an int.

Query Syntax

:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LEADing?

Description

Enters the minimum number of leading consecutive identical digits (CID) that are used to define one and zero levels. Use the :MEASure:AMPLitude:DEFine:LEVel command to select that one and zero levels are defined in terms of CIDs. Use :MEASure:AMPLitude:DEFine:LEVel:CIDigits:LAGGing to set the minimum number of lagging CIDs.

The default setting is 1, the minimum setting is 0, and the maximum setting is 50.

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.