:MEASure:AMPLitude:DEFine:RINoise:DEFinition
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:RINoise:DEFinition {LEGacy | IEEE}
Query Syntax
:MEASure:AMPLitude:DEFine:RINoise:DEFinition?
Description
Configures the RIN measurement (:MEASure:AMPLitude:RINoise) to be based either on FlexDCA's Legacy algorithm or the IEEE 802.3 specification. Click here for the RIN equations. The result of the IEEE based measurement is approximately 6 dB greater than FlexDCA's legacy measurement. Legacy is the default selection.
Additional definitions for the RIN measurement:
:MEASure:AMPLitude:DEFine:RINoise:TYPeto base the measurement on the one level or an OMA measurement.:MEASure:AMPLitude:DEFine:RINoise:UNITsto select the measurement units.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Requires FlexDCA revision A.05.61 and above.