:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LAGGing
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LAGGing <digits>
<digits> is an int.
Query Syntax
:MEASure:AMPLitude:DEFine:LEVel:CIDigits:LAGGing?
Description
Enters the minimum number of lagging consecutive identical digits (CID) that are used to define one and zero levels. Use the :MEASure:AMPLitude:DEFine:LEVel command to select that one and zero levels are defined in terms of CIDs. Use :MEASure:AMPLitude:DEFine:LEVel:CIDigits:LEADing to set the minimum number of leading CIDs.
The default setting is 1, the minimum setting is 0, and the maximum setting is 50.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.