:MEASure:AMPLitude:DEFine:RNCValue:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:AMPLitude:DEFine:RNCValue:LEVel{0|1|2|3} <RN compensation>

<RN compensation> is an double.

Query Syntax

:MEASure:AMPLitude:DEFine:RNCValue:LEVel?

Description

Enters a measured RN compensation value for the specified logic level. The default value is 0V. For NRZ signals, select logic level 0 (zero) or 1. For PAM4 signals, select logic level 0 (zero), 1 (one), 2, or 3. Use the :MEASure:AMPLitude:DEFine:RNComp command to turn RN compensation on.

NRZ Waveform
PAM4 Waveform

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.

Requires FlexDCA revision A.05.60 and above.