:MEASure:AMPLitude:DEFine:RINoise:UNITs

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:AMPLitude:DEFine:RINoise:UNITs {DBHZ | DECibel}

Query Syntax

:MEASure:AMPLitude:DEFine:RINoise:UNITs{?

Description

Selects the method of normalizing a Relative Intensity Noise (RIN) measurement (:AMPLitude:RINoise). The following arguments can be used:

DECibel
Normalize the RIN value to the equivalent noise bandwidth of the sampling channel. Select this argument if the input channel has an optical reference filter.
DBHZ
Select this argument if the channel does not have a filter or the filter is not on. This is the default argument.

Additional definitions for the RIN measurement:

Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.